Supplementary designations - Suffixes

Suffixes are used to identify designs or variants which differ in some way from the original design, or which differ from the current standard design. The suffixes are divided into groups and when more than one special feature is to be identified; suffixes are provided in the order shown in the scheme in fig 1.
The most commonly used suffixes are listed in the following. Note that not all variants are available.
SKF logo