Protection against contamination

The environment in which power tools typically are used can be highly contaminating. This require solutions that will keep the dust outside and prevent the oil from the gearbox leaking into the motor.

SKF help find solutions to prolong the life of tools in such an environment.


SKF logo