Ordering information

For SNL housings in the 30, 31 and 32 series, each of the following items must be ordered separately:

  • housing
  • seals
  • end cover
  • locating rings
  • bearing
  • adapter sleeve

Order example

Two plummer block housings with labyrinth seals are required for two 23036 CCK/W33 bearings on H 3036 adapter sleeves. One housing will accommodate the non-locating bearing at the end of the shaft. The other housings will accommodate the locating bearing and a through shaft.

The following items should be ordered (in addition to the bearings and adapter sleeves):

  • 2 housings SNL 3036
  • 3 labyrinth seals TS 36
  • 1 end cover ETS 36
  • 2 locating rings FRB 17/280

SKF logo