Angular contact spherical plain bearings

When the resultant load (fig. 1) is constant in magnitude, then use

P = y Fr

where
P=equivalent dynamic bearing load [kN]
Fr=radial component of the load [kN]
y=load factor that depends on the ratio of the axial to the radial load Fa/Fr (diagram 1)
SKF logo