External seals

For bearing arrangements where the effectiveness of the seal under specific operating conditions is more important than space considerations or cost, there are several possible seal types to choose from.
For seals that are not supplied by SKF, the information provided here should be used as a guideline only. Make sure to understand the seal’s performance criteria before incorporating that seal into an application. SKF does not accept liability for the performance of any products not supplied by SKF.
SKF logo