SKF.comHomeFind contact informationHelp
SKF.com
SKF product catalogueIndustriesServicesLibraryAbout SKF
News & EventsInvestorsSustainabilityCareer at SKFGroup sites worldwide
Detailed search »

SKF.com / SKF @ptitude Exchange / Focus Area / Reliability Engineering /  Print this page RSS

Sensors & Online Systems

Relevant to all technologies - systems (e.g. @ptitude) use process data as well as vibration data.
 

Users seeking information of this kind are also referred to the SKF Inquire knowledge database, which hosts a collection of application notes and in-depth support articles, as well as answers to frequently asked questions (FAQ). Applications notes and FAQs are free to download. You can find this additional information by clicking the link below.

 
SKF Inquire  

The following relevant items can be found in this area of @ptitudeXchange.

 
Filter these results on
industry
asset type
 
Page:  1(2)
Results:  1-10  of 20  items
Pages:  1  2  << Prev  | Next >>
Added Safety For Today's Railway Industry
Railways, especially those operating mainline passenger and high-speed services, need to be run safely, reliably and efficiently. At the same time, railway operators seek competitive, cost effective solutions. SKF has worked closely with the railway...
 
Centralized Real-Time Oil Condition Monitoring
The importance of clean and dry oil can not be over-stated. Particle count data and water/humidity levels are an invaluable part of any proactive monitoring program. It is important to ensure abrasive wear problems are minimized, and water related...
 
Continuous Moisture Measurement in Lubricating Oil
Moisture measurement in lubricating oil is classically carried out in the laboratory with a Karl Fischer titrator.
 
Fault Detection for Mining and Mineral Processing Equipment
Fault detection techniques have been developed for use in the mining, minerals processing and cement industries. This is a cost-effective solution, under the SKF Copperhead system concept, for the detection of potentially costly machinery faults that...
 
Getting the Inside View of Bearing Loads, Thanks to a Little Touch of Magic
The more engineers can understand what types of loads, stresses and strains bearings experience during operation in real conditions, the better the bearings can...
 
Integration of Diagnostic Sensors for Intelligent Filtration
As research and training have improved the understanding of the damaging effects of contamination in oil, more lubricant users have focused on and expanded existing filtration efforts.
 
Integration of Vibration Signals
Integration results from the physical and mathematical relationship between acceleration, velocity, and displacement units of measure for machinery vibration. Here we outline the case for and against
 
Monitoring Gearboxes With Magnetic Plugs
In early 2001, the average rebuild cost for J.R. Simplot Co.�s Caterpillar 785 haul truck differentials and final drives was $2.11 per hour of operation. By 2003, the average cost had dropped to $1.36 per hour of operation and the mine�s maintenance...
 
New Sensor Solutions for Railways
Harmonization of European railway operations is now well under way, with the promise of advanced control systems that offer improved safety and reliability. The European Train Control System (ETCS) is a ...
 
On-Line Wear Debris Monitoring Technologies - What Works and Why
Wear debris analysis is essential to effectively gauging machinery life. When machine components begin to wear, the evidence can usually be found in the lubricant flowing through the machine. For example, as parts undergo sliding, fatigue or creep,...
 
My SKF.com
Register here »
Email address:       Help »
Password: 
Forgot password »
Select language
Subscriptions
SKF @ptitude Exchange
Terms and ConditionsPrivacy PolicySite ownershipSite Map