SKF.comCasaRicerca informazioni sui contattiGuida
SKF.com
Catalogo dei prodotti SKFIndustrieServiziBibliotecaInformazioni su SKF
NotizieInvestitoriSviluppo sostenibileLavora in SKFSiti del gruppo nel mondo
Ricerca dettagliata »
SKF.com / Prodotti / Catalogo tecnico interattivo / Cuscinetti volventi /
Cuscinetti a rulli cilindrici / Cuscinetti ad una corona di rulli cilindrici /
Print this page
Single row cylindrical roller bearings
Dynamic axial load carrying capacity

Single row cylindrical roller bearings with flanges on both the inner and outer rings can support axial loads in addition to radial loads. Their axial load carrying capacity is primarily determined by the ability of the sliding surfaces of the roller end / flange contact to support loads. Factors having the greatest effect on this ability are the lubricant, operating temperature and heat dissipation from the bearing.

Calculating the dynamic axial load carrying capacity
Under normal operating conditions the axial load carrying capacity can be estimated using the equations below. Conditions that are considered typical for normal bearing operation are:

a certain temperature gradient
There is a difference of 60 °C between the bearing operating temperature and the ambient temperature.
a specific heat loss from the bearing
There is a flow of 0,5 mW/mm2 °C; with reference to the bearing outside diameter surface (A = π D B).
adequate lubrication
A viscosity ratio κ ≥ 2 is required (see the section "Lubrication conditions - the viscosity ratio κ"). For grease lubricated applications, the viscosity of the base oil in the grease may be used. If κ is less than 2, friction and wear will increase. These effects can be reduced at low speeds, for example, by using lubricants with AW (anti-wear) or EP (extreme pressure) additives. In grease lubricated applications where axial loads act for long periods, the bearings should be relubricated frequently with a grease that has good oil bleeding properties at normal operating temperature (> 3% according to DIN 51 817).
sufficient radial load
The value of the radial load should be at least twice the value of the axial load. A lower ratio (axial versus radial load) is possible, but should be checked by the SKF application engineering service.
limited misalignment
Where misalignment between the inner and outer rings exceeds 1 minute of arc, the action of the load on the flange changes considerably. Therefore the safety factors included in the guideline values may be inadequate. In these cases, contact the SKF application engineering service.

For bearings with a heat emitting reference surface area Ar ≤ 50 000 mm2, the permissible axial load can be calculated with sufficient accuracy from

Fap = k1 C0 104 / (n (d + D)) - k2 Fr

For bearings with a heat emitting reference surface area Ar > 50 000 mm2, the permissible axial load can be calculated with sufficient accuracy from

Fap = k1 C0 2/3 7,5 × 104 / (n (d + D)) - k2 Fr

When circulating oil lubrication provides efficient cooling, the permissible axial load can be raised by

ΔFap = k1 ΔTs Vs 15 × 104 / (n (d + D))
where
Ar = heat emitting reference surface area in accordance with ISO 15312:2003
= π B (D + d) [mm2]
Fap = permissible axial load [kN]
ΔFap = raise for permissible axial load due to cooling [kN]
C0 = basic static load rating [kN]
Fr = actual radial bearing load [kN]
n = rotational speed [r/min]
d = bearing bore diameter [mm]
D = bearing outside diameter [mm]
B = bearing width [mm]
ΔTs = temperature difference between oil inlet and outlet [°C]
Vs = oil flow through the bearing [l/min]
k1 = a factor
= 1,5 for oil lubrication
= 1 for grease lubrication
k2 = a factor
= 0,15 for oil lubrication
= 0,1 for grease lubrication

The values for the permissible load Fap obtained from the equations are valid for a constant and continuous axial load provided there is an adequate supply of lubricant to the roller end / flange contacts. Where axial loads act only for short periods, the values can be multiplied by 2. For shock loads the values can be multiplied by 3, provided the following limits relative to flange strength are not exceeded. A short period can last anywhere from several seconds to a few minutes. It is characterized by a temperature spike of not more than 5 °C after which time the bearing returns to normal operating temperature. As a rule of thumb, a short period is considered as the time it takes for the bearing to make 1 000 revolutions. Values calculated according to the above equations are not hard limits. If higher axial load carrying capacity than calculated is required, contact the SKF application engineering service for detailed analysis.

Axial load limit relative to flange strength
To avoid the risk of flange fracture, the constantly acting axial load applied to the bearings should never exceed

Famax = 0,0045 D1,5 (bearings in the 2 Diameter Series)

or

Famax = 0,0023 D1,7 (bearings in other Dimension series)

where
Famax = maximum constantly acting axial load [kN]
D = bearing outside diameter [mm]

Where axial loads act only for short periods, the values for Famax can be multiplied by a factor of 2 while shock loads can be multiplied by a factor of 3.

Requirements for abutments
In applications where single row cylindrical roller bearings are subjected to heavy axial loads, axial runout and the size of the abutment surfaces of adjacent components can affect flange load and running accuracy. To obtain an even flange load and provide proper running accuracy, use the values provided in the table. For the diameter of the abutment surfaces, SKF recommends supporting the inner ring at a height corresponding to half the flange height (fig).

das = 0,5 (d1 + F)

where
das = shaft abutment diameter [mm]
d1 = inner ring flange diameter [mm]
F = inner ring raceway diameter [mm]
 
Dati sui prodotti
 
Cuscinetti a rulli cilindrici
 Cuscinetti ad una corona di rulli cilindrici
 Varianti dell'esecuzione
 Cuscinetti con dimensioni in pollici
 Anelli reggispinta
 Cuscinetti senza anello interno o senza anello esterno
 Esecuzioni speciali
 Cuscinetti SKF Explorer
 Dimensioni
 Tolleranze
 Gioco interno radiale
 Gioco interno assiale
 Disallineamento
 Spostamento assiale
 Influenza della temperatura di funzionamento sul materiale dei cuscinetti
 Gabbie
 Carico minimo
 Capacità di carico dinamico assiale
 Carico dinamico equivalente sul cuscinetto
 Carico statico equivalente sul cuscinetto
 Appellativi supplementari
 

My SKF.com

Registrarsi qui »
Indirizzo e-mail:       Guida »
Password: 
Password dimenticata »
Selezionare la lingua
Vai al sito locale
News dal Gruppo 
SKF Half-year report 2010
(2010-07-22, 17:23)
Inaugurata la SKF Solution Factory francese
(2010-06-24, 15:08)
S-OIL raggiunge gli obiettivi strategici con il contributo SKF
(2010-05-25, 15:21)
[it]More news»
Termini e condizioni legaliINFORMATIVA SULLA TUTELA DEI DATI PERSONALIProprietà del sitoMappa del sito