|
As mentioned in the introduction of the grease lubrication
section, the bearing should initially be completely filled,
while the free space in the housing should be partly filled.
Depending on the intended method of replenishment, the
following grease fill percentages for this free space in the
housing are recommended:
| – |
40% when replenishing is
made from the side of the bearing ( fig 1); |
| – |
20% when
replenishing is made through the annular groove and
lubrication holes in the bearing outer or inner ring
( fig 2). |
Suitable quantities for replenishment from the side of a
bearing can be obtained from
Gp = 0,005 D B
and for replenishment through the bearing outer or
inner ring from
Gp = 0,002 D B
| where |
| Gp
|
= |
grease
quantity to be added when replenishing, g |
| D |
= |
bearing
outside diameter, mm |
| B |
= |
total bearing width (for
thrust bearings use total height H), mm |
To facilitate the supply of grease using a grease gun, a
grease nipple must be provided on the housing. If contact
seals are used, an exit hole in the housing should also be
provided so that excessive amounts of grease will not build
up in the space surrounding the bearing ( fig 1) as this might
cause a permanent increase in bearing temperature. The exit
hole should be plugged when high-pressure water is used for cleaning.
The danger of excess grease collecting in the space
surrounding the bearing and causing temperature peaks, with
its detrimental effect on the grease as well as the bearing,
is more pronounced when bearings operate at high speeds. In
these cases it is advisable to use a grease escape valve
rather than an exit hole. This prevents over-lubrication and
allows relubrication to be performed while the machine is in
operation. A grease escape valve consists basically of a
disc that rotates with the shaft and which forms a narrow
gap together with the housing end cover ( fig 3). Excess and used
grease are thrown out by the disc into an annular cavity and
leaves the housing through an opening on the underside of
the end cover. Additional information regarding the design
and dimensioning of grease escape valves can be supplied on request.
To be sure that fresh grease actually reaches the bearing and
replaces the old grease, the lubrication duct in the housing
should either feed the grease adjacent to the outer ring
side face ( fig 1 and
fig 4) or, better
still, into the bearing. To facilitate efficient lubrication
some bearing types, e.g. spherical roller bearings, are
provided with an annular groove and/or lubrication holes in
the outer or inner ring ( fig 2 and
fig 5).
To be effective in replacing old grease, it is important that
grease is replenished while the machine is operating. In
cases where the machine is not in operation, the bearing
should be rotated during replenishment. When lubricating the
bearing directly through the inner or outer ring, the fresh
grease is most effective in replenishment; therefore, the
amount of grease needed is reduced when compared with
relubricating from the side. It is assumed that the
lubrication ducts were already filled with grease during the
mounting process. If not, a greater relubrication quantity
during the first replenishment is needed to compensate for
the empty ducts.
Where long lubrication ducts are used, check whether the
grease can be adequately pumped at the prevailing ambient temperature.
The complete grease fill should be replaced when the free
space in the housing can no longer accommodate additional
grease, e.g. approximately above 75% of the
housing free volume. When relubricating from the side and
starting with 40% initial fill of the housing, the
complete grease fill should be replaced after approximately
five replenishments. Due to the lower initial fill of the
housing and the reduced topping-up quantity during
replenishment in the case of relubricating the bearing
directly through inner or outer ring, renewal will only be
required in exceptional cases.
|