|
V-ring seals are mounted on shafts and their thin, tapered
lip seals against a surface (counterface) at right angles to
the shaft ( fig 1a). No special demands are placed on the surface
finish of the shaft seat and the V-rings act as flingers
( fig 1b), since they have an interference fit on the shaft
and rotate with it. Misalignment of the shaft with respect
to the counterface ( fig 1c) can be tolerated and V-rings also provide reliable
sealing if the shaft is out-of-round or rotates
eccentrically ( fig 1d). It should be remembered when using V-rings that
the amount by which the shaft can be displaced axially is
governed by the permissible displacement of the V-ring
relative to its counterface.
V-rings are made entirely of elastomer without fabric or
sheet metal reinforcement. They are, therefore, particularly
easy to install. They can be stretched and, depending on
size, can be pushed over other components of the
arrangement, e.g. flanges, pulleys or even housings. This is
a very valuable characteristic, especially in the case of repairs.
|