|
Solid Oil consists of a polymer matrix, which is saturated
with lubricating oil.
The polymer material has a structure with millions of
micro-pores, which hold the lubricating oil. The pores are
so small that the oil is retained in the material by surface
tension. Oil represents an average of 70% by
weight of the material.
The oil used as standard is very high quality synthetic oil,
which meets the needs of most applications.
The oil-filled polymer material is moulded into the bearing.
A very narrow gap will form around the rolling elements and
raceways during the moulding process, enabling the bearing
components to rotate freely. The oil, which seeps into the
gap, provides good lubrication for the bearing right from
the start. Solid Oil completely fills the internal space in
a bearing and encapsulates the cage and rolling elements.
Solid Oil uses the cage as a reinforcement element and
rotates with it.
Solid Oil keeps the oil in position and brings more oil to
the bearing than grease. A metallic surface sliding against
Solid Oil is provided with an even and consistent oil film.
A moderate increase in temperature causes oil to be pushed
towards the surface of the polymer matrix, as the thermal
expansion of the oil is greater than that of the polymer
matrix. The viscosity of the oil also decreases with
increasing temperature. When the bearing stops running, the
polymer matrix reabsorbs excess oil.
In addition, Solid Oil is environmentally friendly and keeps
contaminants out of the bearing, even without seals ( fig 2). However, for
those applications where very good contamination exclusion
is needed, the use of bearings with Solid Oil and integral
contact seals is recommended. But in all cases maintenance
will be unnecessary because no relubrication is needed.
|