SKF.comHomeFind contact informationHelp
SKF.com
SKF product catalogueIndustriesServicesLibraryAbout SKF
News & EventsInvestorsSustainabilityCareer at SKFGroup sites worldwide
Detailed search »

SKF.com / Services /   
Remanufacturing Services

Bearing remanufacturing can result in a significant reduction of CO2 emissions compared to the production of a new bearing as it requires up to 90% less energy than producing a new bearing. By extending the service life of bearings, the process avoids the scrapping of components and the unnecessary use of natural resources.

SKF has decades of experience in bearing remanufacturing. All work is performed at dedicated state-of-the-art SKF remanufacturing service centres in a global network by specialists to rigorous SKF specifications. The work begins with cleaning, degreasing and disassembling the bearings. All components are then inspected. From this inspection, a detailed bearing analysis report is issued. Bearings that are not damaged beyond repair can be restored using appropriate procedures that can include polishing, grinding and component replacement. In fact, a bearing with more than 30% left of its calculated service life can be worth remanufacturing. As a result, the cost savings through remanufacturing could be substantial.

 
My SKF.com
Register here »
Email address:       Help »
Password: 
Forgot password »
Select language
Go to location

More Information

Related Electronic Services:

SKF @ptitude Exchange>>

Interactive Engineering Catalogue >>

SKF.com/Mount >>

 
Terms and ConditionsPrivacy PolicySite ownershipSite Map