SKF.comHomeFind contact informationHelp
SKF.com
SKF product catalogueIndustriesServicesLibraryAbout SKF
News & EventsInvestorsSustainabilityCareer at SKFGroup sites worldwide
Detailed search »

SKF.com / SKF Care / Environmental Care / Climate strategy /  Print this page 

Target


Carbon dioxide emissions reduction

 

SKF's monitoring and reporting of greenhouse gas emissions are carried out in accordance to the Greenhouse Gas (GHG) Protocol developed by the World Business Council on Sustainable Develeopment (WBCSD) and the World Resource Institute (WRI). The Protocol characterizes an organization's greenhouse gas inventory into three scopes, as explained in the diagram below.

 

SKF has voluntarily reported all direct and some indirect CO2 emissions resulting from manufacturing operations since 2002. The first CO2 emission reduction target was defined to aim for a 10% reduction by 2007 (compared with 2002). This target was successfully accomplished in 2005 with a 13% reduction in CO2 emissions, despite production volume increased.

 

Hence, a new target was defined in 2006 to achieve annually a minimum 5% reduction irrespective of production volume increases.

 

SKF reached an absolute reduction of 50,000 tonnes CO2 emissions, or 9.1% compared to the 2007 total, surpassing the target by some 4 percentage point. It is worth noting that the total Group's CO2 emissions from Q1 to Q3 2008 were reduced by more than 5% compared to the same quarters of 2007, despite higher production volumes.

 

The close correlation between manufacturing production and energy use achieved during this period is an indication that the energy management approach applied throughout the company is operating successfully.

 
My SKF.com
Register here »
Email address:       Help »
Password: 
Forgot password »
Select language
Go to location

More Information

Contact me
Terms and ConditionsPrivacy PolicySite ownershipSite Map