Module cookie pe site-ul web SKF

Folosim module cookie pentru a ne asigura că vă oferim cea mai bună experiență pe site-urile și aplicațiile noastre web. Continuând fără schimbarea setărilor browser-ului, presupunem că vă oferiți acordul de a primi module cookie. Totuși, puteți să modificați setările modulelor cookie ale browser-ului în orice moment.

OE expertise at SKF

Innovation and technology that benefit the independent aftermarket

 

SKF is a strategic partner to major car manufacturers worldwide. Its original equipment (OE) products are designed specifically for a certain customer and a particular application.

The in-depth involvement, innovative know-how and experience acquired while collaborating with OE manufacturers is transferred throughout the business, and ensures SKF is able to provide high-quality components with original specifications for customers in the independent automotive aftermarket.

Some examples of OE partnerships - Cars:

  • Volvo Car Corporation
    Wheel hub bearing units for the next generation of premium vehicles. Optimized for lower weight and high performance seals with less friction, to reduce the vehicle weight, without having a negative impact on performance or comfort.
  • Tesla Motors
    Energy efficient, deep groove ball bearings and hybrid (ceramic) bearings for the electric motor and gearbox.
  • Audi
    Wheel hub bearing units designed to fit a range of vehicles, from compacts to SUVs, using Audi’s new modular MLB Evo-platform and optimized solutions for a more efficient transmission.
  • FCA
    Wheel hub bearing units for the front and rear wheels to optimize performance and quality for different models under the FCA brand.
  • Volkswagen
    High performing, high quality wheel hub bearing units and MacPherson suspension bearing units.
  • PSA
    High performing high quality bearings and seals for a number of PSA models.
  • Hyundai
    MacPherson suspension bearing unit with improvement in sealing and stiffness with a robust seal and a steel inserted washer.

Some examples of OE partnerships - Commercial vehicles:

  • Scania
    High pressure valve stem seals designed to withstand the extreme pressure levels generated by modern down-sized and turbo-boosted engines. The solution’s reliability and high performance levels help contribute to improved truck engine efficiency.
  • Daimler
    Gear bearing unit solution for heavy duty engines to accommodate higher loads for special purpose vehicles like concrete lorries, fire trucks or crane trucks.
  • MAN
    The truck-matched wheel end units are quicker to assemble and provide a lower total cost of ownership, through extended maintenance intervals.

SKF Racing - Bringing innovation to the track

Advanced engineered solutions and services to racing teams throughout the world

SKF has been involved in racing for nearly a century and collaborates with the most demanding and prestigious customers in the sector. Few, if any, settings offer a more intense and exacting test environment than top-class racing. Knowledge gained from SKF’s cutting edge product development for the racing industry is used to offer new solutions to automotive clients with high volume manufacturing as well as customers in the independent automotive aftermarket.
From the classic blue Bugatti’s of the 1930’s with roller bearing central crankshaft support, to the sophisticated and highly complex Grand Prix thoroughbreds of today, SKF’s technology has kept gearboxes shifting, camshafts revolving and wheels turning.

Racing sponsorships

Dovizioso_2015
Ferrari_00P5785
brad-keselowski

Scuderia Ferrari
SKF’s cooperation with Scuderia Ferrari spans almost 70 years – the longest uninterrupted partnership in the history of Formula One.
The partnership includes the supply of advanced bearing and sealing solutions, condition monitoring devices as well as engineering services with a special focus on supporting them develop energy recovery systems.
The current Formula One model has more than 150 SKF components in its wheels, engine, gearbox and suspension.
Other technical partners within Formula One include Renault F1, the Red Bull Racing team and Scuderia Toro Rosso as well as WilliamsF1 and McLaren.


Ducati
The cooperation between SKF and Ducati began in the forties. Since then, the two companies have overcome the difficulties and challenges demanded by the fast developing technologies in the world of two-wheelers.
With Ducati in the World Superbike Championship the partnership has been consolidated even further. The story has continued with new Ducati Desmosedici adventure in the Moto GP world championship.


Nascar
For almost two decades, SKF has been both a technical partner and sponsor for NASCAR.
The partnership with Penske Racing enables SKF to test products under the harshest conditions within both the NASCAR and IndyCar series.

Betamotor
The SKF-Betamotor partnership began in the sixties and for over 50 years motocross, enduro and trial motorcycles have been equipped with SKF products.

SKF logo