Cooling and roll-out tables

Bearing challenges at the end of the casting line

The end of the casting process presents high temperature challenges of its own. To avoid structural transformation of the product, water is not used to cool the steel in this final casting stage. For bearings, this means exposure to higher radiant heat - a challenge often addressed with water-cooled housings or high-temperature lubricants.

Meet them with SKF
SKF offers several solutions that can help bearings handle the high temperatures found on cooling beds and roll out tables. Follow the links below to see how SKF solutions can help deliver more uptime and less maintenance at the end of the casting line.

Решения SKF для охладительных и вытяжных столов

SKF logo