Turbomachinery and Pump Symposia

September 15 - 17, 2015

Location: Houston, TX
Venue: George R. Brown Convention Center
Booth number: 1153

Event website: http://pumpturbo.tamu.edu/

Short description of event:
The Turbomachinery and Pump Symposia is held to promote professional development, technology transfer, peer networking, and information exchange among industry professionals. The event is led by engineers with vast experience in the petrochemical, process, chemical, utility, contractor, and consulting fields, along with manufacturers of rotating equipment and fluid-handling equipment from around the world. The event features lectures, tutorials, case studies, discussion groups, and short courses, as well as exhibits of the latest services and full-sized equipment.
Short description of SKF’s part in the event:
Alemite will have a 10 x 20 display at this show and will feature the Carbon Shield oil mist unit that is used extensively in the oil and gas industry.

SKF logo