Sir H K D H Bhadeshia

Harry Bhadeshia
Harry Bhadeshia is a metallurgist and Tata Steel Professor of Metallurgy in the Department of Materials Science & Metallurgy at the University of Cambridge.

Bhadeshia obtained his PhD in 1980 at Cambridge, and has been a part of the academic staff since then. He is the author of several books and more than 500 published papers in the field of metallurgy.

Since 2009, Bhadeshia has headed up the SKF University Technology Centre, a cooperation between SKF and the University of Cambridge to conduct research in the field of physical metallurgy of bearing steels.

Watch the video on the main Let's Talk Future Materials page where Harry Bhadeshia was a guest speaker.
SKF logo