SKF Agri Hub

Reference cases

A farmer’s testimony
"My farm requires 40 days tillage a year – 30 in spring to prepare for the maize and 10 in autumn to prepare for the wheat. With the new solution there is no need to wash and lubricate the discs and I save half an hour a day. The work is done more quickly and easily. We drive at more than 20 km an hour and I have seen an improvement in the way the land is worked: with the old harrow the top speed was 7 or 8 km an hour. The old 2,5 metre wide harrow worked one hectare an hour, the new machine, which is still 2,5 metre wide covers two and a half hectares an hour. The old 20-disc harrow required a 20 kilogram can of grease each year, with this new solution I’ve eliminated greasing and washing. In my job I’m in contact with nature every day and I’m pleased that with the new SKF solution I’m not polluting the land with grease anymore."

www.skf.com | Terms and Conditions | Privacy Policy | Site ownership