Cookies on the SKF website

SKF uses cookies on our websites to align the information shown as closely as possible to our visitors’ preferences, such as country and language choices.

Will you accept SKF cookies?

Information about Cookies

Cookies
SKF web sites use cookies. A cookie is an element of data that a web site can send to your browser, which may then store it on your system. SKF uses cookies to coordinate the information on our web sites as closely as possible to the preferences of you as a visitor (such as country and language choices). Further, cookies help to tailor the information the web site will provide to you upon a return visit. Items such as a username, should you have registered with this web site, may be stored via a cookie.

SKF cookies
On SKF's web sites, both transient and persistent cookies are used. With transient cookies we refer to cookies that are only kept in memory within the lifespan of the user's session with the site. These cookies are not persisted to the end user's system.

Persistent cookies make it possible for our web site to recognize you whenever you return to our web site so that the settings you have made during previous visits are recognized so you don't need to re-set them ever visit. Persistent cookies are persistently stored on the client system  (hard drive or elsewhere), the lifetime of these cookies can span from a few seconds to several years. Examples of where SKF web sites use persistent cookies are to remember country/language selections; helping with collecting statistics; and for remembering if the user already has responded to an on line survey.

Options
If you don't wish to accept cookies from the SKF web site you can: leave this web site, or configure your browser to either notify you when you receive a cookie (giving you the chance to decide whether to accept it) or to block all or certain categories of cookies. The browser can also delete previously stored cookies. Please see your browser's help facility for information on setting how cookies are handled. Even if you have turned off the setting in your browser that allows the use of cookies, you can still visit most of the sections available at SKF's web sites.

SKF logo