Cookies on the SKF website

SKF uses cookies on our websites to align the information shown as closely as possible to our visitors’ preferences, such as country and language choices. Will you accept SKF cookies?

Remanufacturing services

Bearing remanufacturing can result in a significant reduction of CO2 emissions and require as much as 90% less energy compared to the production of a new bearing.  By extending the service life of bearings, the process avoids the scrapping of components and the unnecessary use of natural resources.

SKF has decades of experience in bearing remanufacturing. All work is performed at dedicated state-of-the-art SKF remanufacturing service centres according to rigorous SKF specifications by a global network of specialists. The work begins with cleaning, degreasing and disassembling the bearings. All components are then inspected. From this inspection, a detailed bearing analysis report is issued. Bearings that are not damaged beyond repair can be restored using appropriate procedures that can include polishing, grinding and component replacement. In fact, a bearing with more than 30% left of its calculated service life can be worth remanufacturing. As a result, the cost savings through remanufacturing can be substantial.
SKF logo