Cookies on the SKF website

We use cookies to ensure that we give you the best experience on our websites and web applications. By continuing without changing your browser settings, we assume you give your consent to receive cookies. However, you can change your browser cookie setting at any time.

Contact seals

Contact seals (fig. 1) are generally very reliable. Their effectiveness, however, depends on a number of factors including:
  • the seal design
  • the seal material
  • the contact pressure
  • the surface finish of the seal counterface
  • the condition of the seal lip
  • the presence of lubricant between the seal lip and counterface
The contact pressure (fig. 1) can be produced either by:
  • the resilience of the seal, resulting from the elastic properties of the seal material (a)
  • the designed interference between the seal and its counterface (b)
  • a force exerted by a garter spring incorporated in the seal (c)
Friction between the seal lip and counterface can generate a significant amount of heat. As a result, these seals have circumferential speed limits. They are also susceptible to mechanical damage as a result of improper mounting, or by solid contaminants. To protect the seal from the damage caused by solid contaminants, a non-contact seal is typically placed in front of a contact seal.
SKF logo