Cookies on the SKF website

SKF uses cookies on our websites to align the information shown as closely as possible to our visitors’ preferences, such as country and language choices.

Will you accept SKF cookies?

Ordering information

For SNL housings in the 30, 31 and 32 series, each of the following items must be ordered separately:

  • housing
  • seals
  • end cover
  • locating rings
  • bearing
  • adapter sleeve

Order example

Two plummer block housings with labyrinth seals are required for two 23036 CCK/W33 bearings on H 3036 adapter sleeves. One housing will accommodate the non-locating bearing at the end of the shaft. The other housings will accommodate the locating bearing and a through shaft.

The following items should be ordered (in addition to the bearings and adapter sleeves):

  • 2 housings SNL 3036
  • 3 labyrinth seals TS 36
  • 1 end cover ETS 36
  • 2 locating rings FRB 17/280

SKF logo