Cookies on the SKF website

SKF uses cookies on our websites to align the information shown as closely as possible to our visitors’ preferences, such as country and language choices.

Will you accept SKF cookies?

Checking the static load carrying capacity

For dynamically loaded bearings, where the equivalent static bearing load P0 is known, it is advisable to check that the static load carrying capacity is adequate using

Static load carrying capacity

If the s0 value obtained is less than the recommended guideline value (table 1), a bearing with a higher basic static load rating should be selected.
SKF logo