Cookies on the SKF website

SKF uses cookies on our websites to align the information shown as closely as possible to our visitors’ preferences, such as country and language choices.

Will you accept SKF cookies?

Angular contact spherical plain bearings

When the resultant load (fig. 1) is constant in magnitude, then use

P = y Fr

where
P=equivalent dynamic bearing load [kN]
Fr=radial component of the load [kN]
y=load factor that depends on the ratio of the axial to the radial load Fa/Fr (diagram 1)
SKF logo