Cookies on the SKF website

SKF uses cookies on our websites to align the information shown as closely as possible to our visitors’ preferences, such as country and language choices.

Will you accept SKF cookies?

Internal clearance

Bearing internal clearance (fig. 1) is defined as the total distance through which one bearing ring can be moved relative to the other in the radial direction (radial internal clearance) or in the axial direction (axial internal clearance).

In almost all applications, the initial clearance in a bearing is greater than its operating clearance. The difference is mainly caused by two effects:

  • Bearings are typically mounted with an interference fit on the shaft or in the housing. The expansion of the inner ring or the compression of the outer ring reduces the internal clearance. 
  • Bearings generate heat in operation. Differential thermal expansion of the bearing and mating components influences the internal clearance.
Sufficient internal clearance in a bearing during operation is important. Preload (clearance below zero) is possible for certain bearing types.
To enable selection of the appropriate initial internal clearance to achieve the desired operational internal clearance, bearings are available in different clearance classes. ISO has established five clearance classes for many bearing types. SKF uses designation suffixes to indicate when the bearing internal clearance differs from Normal.
ISO clearance
class
SKF designation
suffix
Internal clearance
-C1Smaller than C2
Group 2C2
Smaller than Normal
Group N-
Normal
Group 3C3
Greater than Normal
Group 4C4
Greater than C3
Group 5C5
Greater than C4

SKF logo