Cookies on the SKF website

We use cookies to ensure that we give you the best experience on our websites and web applications. By continuing without changing your browser settings, we assume you give your consent to receive cookies. However, you can change your browser cookie setting at any time.

Bearings of the TDI configuration

Bearings of this configuration (fig 1) have a double row inner ring with two roller and cage assemblies (double cone) and two outer rings (cups). The two rows of rollers are arranged face-to-face. Normally an intermediate ring is arranged between the two outer rings. This ring is dimensioned so that a certain axial clearance or preload will be obtained.
The bearings are eminently suitable for locating bearing arrangements and are produced by SKF with a cylindrical bore; some sizes are also produced with a tapered bore. For bearing arrangements where the bearings are to be mounted with a loose fit on the shaft or journal, special designs are supplied by SKF. To counteract the disadvantage of a loose fit on the shaft – the inner ring turns on its seat, which can cause damage to the bearing and the seat – these special bearings have a helical groove in the bore and/or lubrication grooves in the side faces of the bearing rings (fig 2). These grooves enable lubricant to be efficiently supplied to the sliding contact surfaces.
Bearings having a large contact angle are a special design of the TDI configuration (fig 3). These bearings have a particularly high axial load carrying capacity and are used primarily as thrust bearings in rolling mill applications. As they are mounted with a loose fit on the roll neck and only subjected to purely axial load, the inner ring has one or more notches in one or both side faces to permit it to be secured and prevent it from turning on its seat. Depending on the application the bearings are supplied with or without an intermediate ring between the two outer rings. They can also be supplied as self-retaining units with a retention sleeve over the outer rings (fig 4).
These self-retaining bearing units with retention sleeve are characterised by high load carrying capacity and simple handling compared with conventional bearings. The outer rings are integrated in the sleeve. The deformation of the outer rings normally resulting from heavy axial loads is considerably reduced by this means and as a consequence the stress distribution in the rolling contacts is more favourable leading to longer life. The axial internal clearance is determined by the sleeve. Preloading by means of springs is not needed. The arrangement design is simplified and thus more economic and mounting is also easier.

SKF produces double row tapered roller bearings of the TDI configuration mainly in the designs described in the following.

TDI design

Bearing with intermediate ring and pressed steel window-type cages (fig 5).

TDI.1 design

Bearing with intermediate ring, pierced rollers and steel pin-type cages (fig 6).

TDIE design

Bearing with inner ring extended at both sides, intermediate ring and pressed steel cages. The inner ring extensions are ground and serve as lands for radial shaft seals (fig 7).

TDIT design

Bearing with tapered bore, taper 1:12, intermediate ring between the outer rings and pressed steel cages (fig 8).

TDIS design

Bearing with large contact angle, intermediate ring between the outer rings and pressed steel cages (fig 9).

TDIS.1 design

Bearing with large contact angle, intermediate ring between the outer rings, pierced rollers and steel pin-type cages (fig 10).

TDIS.2 design

Self-retaining bearing units with large contact angle, outer rings held in a retention sleeve, pierced rollers and steel pin-type cages (fig 11).
SKF logo