Cookies on the SKF website

SKF uses cookies on our websites to align the information shown as closely as possible to our visitors’ preferences, such as country and language choices.

Will you accept SKF cookies?

Designs and variants

Matched bearings arranged face-to-face
  • have load lines that converge toward the bearing axis (fig. 1)
  • can accommodate a limited amount of misalignment
  • can accommodate axial loads in both directions
  • are supplied with an intermediate outer ring spacer as a set
Matched bearings arranged back-to-back
  • have load lines that diverge toward the bearing axis (fig. 2)
  • provide a relatively stiff bearing arrangement
  • can accommodate tilting moments
  • can accommodate axial loads in both directions
  • are supplied with intermediate inner and outer ring spacers as a set
Matched bearings arranged in tandem
  • have load lines that are parallel (fig. 3)
  • share radial and axial loads equally
  • are used when the load carrying capacity of a single bearing is inadequate
  • can accommodate axial loads in one direction only; if axial loads act in both directions, a third bearing must be added and adjusted against the tandem pair
  • are supplied with intermediate inner and outer ring spacers as a set
SKF Explorer bearings
SKF continuously expands its assortment of SKF Explorer bearings. In addition to the existing SKF Explorer matched tapered roller bearings (→ product tables), SKF can also manufacture basic design tapered roller bearings as SKF Explorer bearings, on request. These SKF Explorer tapered roller bearings are identified by the designation suffix PEX.
Cages

SKF matched tapered roller bearings are fitted with one of the cages shown in table 1. The standard stamped steel cage is not identified in the bearing designation. If non-standard cages are required, check availability prior to ordering.

When used at high temperatures, some lubricants can have a detrimental effect on polyamide cages. For information about the suitability of cages, refer to Cages.

SKF logo