Cookies on the SKF website

SKF uses cookies on our websites to align the information shown as closely as possible to our visitors’ preferences, such as country and language choices.

Will you accept SKF cookies?

Bearing mounting and dismounting

Mounting is one of the critical stages of the bearing’s lifecycle. If the bearing is not mounted properly using the correct method and tools, the bearing’s service lifetime will be reduced. Around 16% of all premature bearing failures are a result of poor fitting or using incorrect mounting techniques.

At some point, the bearing will reach the end of its service life and will have to be replaced. Although the bearing may not be used again, it is extremely important to dismount it correctly so that the service life of the replacement bearing is not compromised. Firstly, the use of proper dismounting methods tools will help prevent damage to other machine components, such as the shaft and housing, which are often re–used. Secondly, incorrect dismounting techniques can be hazardous to the operator.

SKF can supply experienced Mechanical Service Engineers using the latest bearing mounting and dismounting equipment and techniques to assist with most bearing jobs.

Click here to go to the SKF Maintenance Products website.

SKF logo