SKF BeyondZero customer solutions
Targeting zero is good. Going beyond zero is better.
SKF BeyondZero is sustainability from the customers' perspective. SKF BeyondZero customer solutions bring significant environmental benefits to our customers in one of the following areas:- Help preserve the balance of the atmosphere.
- Promote efficient and responsible use of land resources.
- Avoid discharges into water.
Some of the products and services included in the SKF BeyondZero customer solutions are presented below:
-
SKF Nautilus
-
-
-
SKF CASM electric cylinders
-
SKF Food Line Y-bearing units
-
SKF Sealed SRB for continuous casting
-
SKF Dry-Lube bearings
-
SKF ConRo
-
SKF Cylinder Lubrication System
-
SKF Tyre Pressure Monitoring System
-
SKF Motor Encoder Sensor-Bearing Unit
-
SKF Rotor Positioning Bearing
-
SKF Rotor Positioning Sensor-Bearing Unit
-
SKF Low Friction Engine Seal
-
SKF StopGo
-
SKF Low Weight Hub Bearing Unit
-
SKF eDrive Ball Bearing
-
SKF Low Friction Hub Bearing Unit
-
High pressure valve stem seal
-
Low friction driveline solutions
-
Low friction X-tracker
-
SKF High Performance Hub Bearing Unit Seal
-
Preload range reduction for hub bearing unit
-
Sealed DGBB for driveline
-
SKF Remanufacturing Services
-
SKF Remanufacturing for Railway
-
SKF high-speed permanent magnet motor system
-
SKF Turbocharger Ball Bearing Unit
-
SKF Flowline
-
SKF Energy Efficient TRB for trucks
-
SKF Bus Door Actuator
-
SKF Extended Life Plain Bearings
-
SKF Solutions to Ocean energy
-
SKF Solutions to Wind energy
-
Electric vehicles
-
SKF LubriLean for Cutting Processes
-
SKF Agri Hub
Inclusions by industry
-
Critieria for inclusion
Solutions within the SKF BeyondZero portfolio must provide significant environmental benefits without serious environmental trade-offs, from a life cycle perspective. They need to address one or more defined environmental challenges, such as, climate change, natural resource use and the avoidance of various types of environmental contamination.
This can be done in one of two ways:- The product or solution can be “Designed for environment”; it provides environmental benefits in its own right through some inherent characteristics (such as low friction or low weight),
- or it can be “Applied for environment”; the product or solution helps to improve the environmental performance of the system (customer application) in which it is applied.
SKFs complete business within the renewable energy industry as well as SKF’s emerging business in the full electric vehicle industry are included in the SKF BeyondZero portfolio under the “Applied for environment” category. These industries are included because it is widely acknowledged that they are technologically critical to reducing fossil fuel use and therefore addressing climate change.
The benefits are derived from a comparison of the environmental performance of SKFs solution to that of a defined baseline.
-
Governance
-
Methodology