Ordering information
SAF and SAW pillow (plummer) blocks are typically supplied as complete kits including housing, seals, bearing, adapter sleeve (or nut and washer) and a standard stabilizing (locating) ring. A complete pillow block is specified by a designation provided in the product tables for:
Optional features can be specified with a prefix and suffixes. If several suffixes are required, put them in alphabetical order.
All pillow block parts can also be supplied separately. Designations for the different parts are listed in the product tables.
Optional components are listed in the product tables and in table 1.
Order example
A shaft with 4 3/16 inch diameter has to be supported by two SAF pillow blocks with 22224 EK spherical roller bearings on an adapter sleeve, one at the shaft end for the non-locating bearing position and one for a through shaft at the locating bearing position. The housings should be sealed with PosiTrac Plus seals.
The following items should be ordered:
- 1 pillow block SAF 22524 TLCY
-
1 pillow block SAF 22524 TLC
The delivery will contain:
- 2 housings SAF 524
- 2 spherical roller bearings 22224 EK
- 2 adapter sleeves with lock nuts SNW 24x4.3/16
- 2 locating rings SR 24-20
- 4 labyrinth rings with O-rings LOR 113
- 3 contact elements B-10724-113
-
1 end plug EPR 14