Cookies sur le site Internet SKF

SKF utilise des cookies sur ses sites Web pour proposer et afficher des informations ciblées et adaptées aux préférences de ses visiteurs, par exemple le choix du pays et de la langue.

cookie_information_popup_text_2[57]

Typical shaft-bearing combinations

SNLN 30 housings can accommodate different shaft-bearing combinations:
Plain shaft with bearing on an adapter sleeve
Housings, appropriate parts and dimensions are listed in the product table (fig. 1).
Stepped shaft with bearing on a cylindrical seat

Housings, appropriate parts and dimensions are listed in the product table.

The bearing is located axially between a shaft shoulder and a spacer sleeve, which is held in place by another component on the shaft (fig. 2). The outside diameter of the sleeve must match the bore diameter of the seal. The spacer sleeve is not supplied by SKF.

Stepped shaft with bearing on an adapter sleeve
When using an SNLN 30 housing for this arrangement (fig. 3), the dimensions of the abutment ring and the spacer sleeve must fit the housing. Abutment rings and spacer sleeves are not supplied by SKF.
Stepped shaft with bearing on a withdrawal sleeve
When using an SNLN 30 housing for this arrangement (fig. 4), the withdrawal sleeve must be located axially on the shaft. This can be done using a spacer sleeve that is held in place by another component. Using a lock nut can be difficult because of the limited space in the housing. The outside diameter of the spacer sleeve must be the same as the shaft abutment diameter, db, (→ product table) and it should be in accordance with the h9Ⓔ tolerance class to fit the seal. The spacer sleeve is not supplied by SKF.
SKF logo