Simulation of dynamic behaviour of rolling bearings
Simulation of dynamic behaviour of rolling bearings
Computer simulation techniques are beginning to make significant progress in understanding what happens in bearings during operation. Dynamic behaviour has represented a significant challenge to software designers because of the complex computing tasks required. Yet many of the problems arise in bearing systems are dyanmic in nature. SKF has developed its own simulation software called BEAST (bearing simulation tool).In verification tests, this has proved to be a valid method of preditcing bearing behaviour under dyanic conditions.BEAST is useful tool for SKF engineers,increasing their understanding of bearing dynamics.It helps to speed up the development process and to provide advanced application support to SKFs customers.