Intelligent gearbox performance management

Facts
Published date:
Format: PDF
Enter promo code

Intelligent gearbox performance management

Dynamic torque measurement has a high potential to optimize drive train performance and reliability by avoiding excessive stress on the components. The accumulated load data can also be used for a sophisticated evaluation of the remaining lifetime. Rotor imbalances can be detected and critical operation points actively prevented. The intelligent gearbox therefore comes equipped with state-of-the-art CMS sensors. All the measured information is enriched with the domain knowledge of ZF as a major global gearbox manufacturer and provided to the customers in a cloud environment. Apart from the basic concept the presentation will also provide inside into actual application data from turbines in the field to demonstrate the potential of the approach.

SKF logo