Reducing operating cost through innovative solutions

Facts
Published date:
Format: PDF
Enter promo code

Reducing operating cost through innovative solutions

Operating costs associated with ‘unscheduled’ maintenance needs can weaken or, oftentimes, pose a significant threaten the financial viability of a project. Traditional repair methods include complete removal of a damaged component, typically the gearbox, using large cranes. Although crane costs (in the US) have come down due to increased competition over time, it is still a large piece of the overall repair cost. RENEW has developed numerous repair methods, tooling and procedures to reduce or eliminate the crane costs all together. Safety and Quality are paramount to the new processes and always our first consideration. Considerable effort goes into R&D, testing and certification of tooling and methods. RENEW has developed numerous methods to perform insitu repairs which has eliminated or reduced the size of crane needed to perform the repair. This presentation will introduce several of these proven methods.

SKF logo