Nor-Shipping
June 02 - 05, 2015
Location: Oslo/Lillestrøm, Norway
Venue: Norges Varemesse/Norway Trade Fairs
Stand #: E 03-19
About Nor-Shipping
Nor-Shipping is one of the leading maritime events and attracts professionals from all over the world. It takes place every two years in Oslo/Lillestrø. The main theme areas of this year´s Nor-Shipping trade show are: IT and navigation; safety and rescue; shipbuilding and repair; maritime services and logistics; and propulsion and machinery.
You can find complete information about the event at the Nor-Shipping website.
Presenting a full marine product portfolio
SKF and SKF Blohm + Voss Industries will be presenting their combined marine product portfolio at the Nor-Shipping trade fair. The theme “Twice the power” will be the red thread through this exhibition.
One example of this is the impressive thruster exhibition model, which will be set up at Nor-Shipping. Visitors can see for themselves the full range of associated products and services with the help of this two metre-plus replica of a thruster. Everything from the bearings, the gear coupling and lubrication system to the SIMPLEX-COMPACT seal and the propeller sleeve will be displayed.
Also on show will be supplementary services such as condition monitoring solutions and alignment services.