Ordering information
SKF housings for paper machines are supplied complete with covers, seals and plugs. The bearings must be ordered separately.
Order examples
Two housings with inch thread dimensions are required for a felt roll assembly – one for a 22218 EK/C3 spherical roller bearing in the locating bearing position, and one for a C 22218 K/C3 CARB toroidal roller bearing in the non-locating bearing position at the end of a shaft. The following items should be ordered (in addition to the bearings):
- 1 SBFN 2218 BFN9
- 1 SBFN 2218 ARAN9
Two housings are required for a drying cylinder assembly – one for a 23144 CCK/C4W33 spherical roller bearing in the locating bearing position, and one for a C 3144 K/C4 CARB toroidal roller bearing in the non-locating bearing position at the end of a shaft. The housings require a special paint that can accommodate special customer requirements. The following items should be ordered (in addition to the bearings):
- 1 SBPN 3144 BF/P..
-
1 SBPN 3144 ARA/P..
Two housings are required for a Yankee cylinder – one for a 230/670 CAK/C084W33 spherical roller bearing in the locating bearing position, and one for a C 30/670 KM/C084 CARB toroidal roller bearing in the non-locating bearing position. The following items should be ordered (in addition to the bearings):
- 1 SDM 30/670 F
- 1 SDM 30/670 RA