Kolačići na web-stranici SKF-a

SKF na svojim web-mjestima koristi kolačiće zbog bolje prilagodbe željenim postavkama korisnika kao što su odabir zemlje i jezika.

Prihvaćate li SKF-ove kolačiće?

Posidonia 2016

Posidonia 2016

June 06 - 10, 2016

Location: Athens, Greece
Venue: Metropolitan Expo
Booth number: Hall 2, stand 2.409

Event website: http://www.posidonia-events.com

Short description of event:
Every two years the Posidonia exhibition is the essential place for serious business at the largest gathering in the shipping calendar.
The trade show provides direct access to Greek shipping and the owners of the largest fleet under the control of any one national group, dominating the newbuilding orderbook and S&P market.

Short description of SKF’s part in the event:
SKF will be presenting its complete Marine product portfolio at the Posidonia 2016 trade show. Bearings, couplings, lubrication systems as well as the Simplex seal range and Turbulo oily water separators will be displayed. Also on show there are marine services such as condition monitoring solutions alignment and on-site machining.

SKF logo