SKF Bearing Select - New

Facts
Format: Web application
Product platform: Bearing, units and housings
SKF Bearing Select Icon online blue

Please, use our new online bearing selection tool, SKF Bearing Select*. SKF Bearing Select will replace the SKF Bearing Calculator as well as the current version of SKF Bearing Select. This new tool has a fully updated, clean and user-friendly interface. Calculation results can be obtained faster and are presented directly near the required input data. SKF Bearing Select has been designed in alignment with the new Bearing Selection Process

Main features:
  • Fast and easy bearing search 
  • Calculation of relevant bearing performance parameters:
    • Rating life
    • Grease life/relubrication interval
    • Lubrication conditions
    • Bearing loads
    • Friction & power loss
    • Frequencies
    • Adjusted reference speed
  • Save projects
  • Automatic report generation 

*SKF Bearing Select is under development, therefore not all functionalities are finalized. For the following calculations, please use the SKF Bearing Calculator
  • Shaft and housing tolerances and resulting fits
  • Calculations for plain bearings, rod-ends, bushings, washers, strips, hybrid bearings, bearings for extreme temperatures. 

For the following calculations, please use the previous version of SKF Bearing Select

  • Two bearings on a shaft
  • Load cycle analysis
Enter promo code
SKF logo